A MAGNAificent performance

03/11/2017

MAGNA3

When Grundfos introduced the MAGNA3 range five years ago, they hoped that consultants and contractors would embrace this flexible range of intelligent, high-efficiency circulators.

Today, having just past the 1,000,000-pump produced milestone, the MAGNA3 is an established firm favourite for a wide range of projects that involve heating, cooling, ground source heat pump systems and domestic hot water applications. In fact, any solution that can benefit from an intelligent high efficiency circulator.

Available in single and twin head options that cover a wide range of duties, specifying the MAGNA3 is straightforward, as the range offers a maximum head of 18m and flow of 70m3/h (140 m3/h for twin head models), and supports 6 to 16 bar system pressure. All of which means the MAGNA3 will be a perfect fit regardless of the project.

To find out more about these pumps as well as the rest of the commercial range from Grundfos visit www.grundfos.co.uk/magna3 - you’ve now got a million more reason to do so.