Grundfos have the shower power

02/02/2018

Grundfos have the shower power

Grundfos Pumps are a specialist shower pump manufacturer who offer a wide range of pumps that are designed to boost the water pressure to a shower or to other bathroom fittings.

With a total of five WRAS approved models in the range, these compact pumps are easy to install and will deliver a pressure range of between 1.5 bar to 6 bar. Plus, whether you require a single a twin impellor, brass or composite design or universal head or positive head operation, Grundfos have all the answers you require.

These products are also part of the Grundfos WIN & EARN loyalty scheme line-up and installers can earn 400 points for every qualifying product they purchase. Simply enrol on the scheme and collect points using the codes from twelve participating pump ranges from the extensive Grundfos family.  Once a minimum of 2,000 points have been accrued, these can be traded in for Amazon vouchers or a range of sports equipment.