Grundfos is at the Center of attention

30/11/2015

In the swim

Center Parcs are already a household name in the UK and Europe and with plans well established to develop the first village near Longford, it looks like they will soon become one in Ireland too.

The brand is synonymous with fun, family activity holidays and their sites currently entertain over 2 million visitors a year in the UK. This means having many leisure pursuits available and one of the most popular revolves around the many water based water based activities they offer. The importance of delivering the key element – water - is something that we at Grundfos are quite expert in.

Because of this, Grundfos were approached by Center Parcs to supply a range of pump solutions to upgrade and maintain the continuity of the water supply at two of the existing facilities. Following consultation, a range of energy efficient pumps including a Hydro MPC-E booster set and a number of SP submersible pumps were supplied along with members of the hard-working Grundfos NBE single-stage standard bloc pump families. With their compact design and low energy usage, these pumps, that are available up to 25 bar, are perfect for dealing with large volume demands.

With a UK turnover of £385m, a 97% occupancy rate and a 96% customer satisfaction rating, Center Parcs cannot leave any aspect of their business simply to chance. This is why the trust they have placed in Grundfos will continue to be repaid through the efficient and effective service that the Grundfos name is synonymous with.





    Facebook Twitter LinkedIn Technorati