Grundfos the over and above pump provider

10/07/2017

Grundfos the over and above pump provider

Mention the name Grundfos and most people will think heating circulators. However, there is much more to Grundfos than this and today they can offer a surprisingly large and sophisticated product portfolio.

Although these include the well-known Grundfos UPS2 and ALPHA3 heating circulator ranges and the SOLOLIFT range of macerators that have become increasingly popular in recent years, today Grundfos can supply a range of additional pump ‘specialists’ that can meet a host of other specific demands, this includes a comprehensive range of shower booster and universal head shower booster pumps.

The latest kid on the block is one that is creating a lot of interest and is the WRAS approved Grundfos SCALA2. Each unit is a fully integrated water booster pump that will provide the perfect water pressure to up to 8 water outlets – even with multiple taps and showers running at the same time. The SCALA2 combines the pump, motor, tank, sensor, drive and non-return valve in one neat package.

So, when you next think of Grundfos, think of them as offering solutions over and above heating circulators. Visit www.grundfos.co.uk to find out more.