Right at home with the Grundfos FireSAFE

01/08/2016

FireSAFE

The Grundfos FireSAFE Domestic range delivers a compact, consumer and installer friendly response to the growing demand for domestic fire suppression systems as well as meeting the recent legislative demands that all new homes in Wales now need to attain.

Designed to ensure flexible installation and easy maintenance, each model in the
Grundfos FireSAFE domestic range complies with BS9251:2014. Each unit comprises of a dedicated controller and Grundfos CM pump mounted in a tamper resistant metal enclosure. The enclosure comes in two sizes, both of which are
dimensioned for easy installation in domestic environments.

This range can be used in a variety of domestic installations including houses, apartments, sheltered and student accommodation, care homes and small hotels. Larger properties could benefit from specifying larger FireSAFE Residential products.

Offering a great range of features such as simple installation and commissioning, a compact size, minimal maintenance, combined with their advanced system controller and in-built self-test makes these the ideal solution in many situations. 

For more details on this and other Grundfos product ranges visit www.grundfos.co.uk





    Facebook Twitter LinkedIn Technorati