Grundfos can take the pressure

09/06/2014

CMB CMBE

Low water pressure can create problems in various domestic and small commercial applications. Fortunately Grundfos have developed a range of solutions that can satisfy the most demanding of requirements by providing a pressurised hot and cold system connected to a Grundfos pressure-boosting pump.

A good example of this is the Grundfos range of single-phase pre-packaged CMB/CMBE booster sets. These booster variants are based around the Grundfos CM stainless steel booster pumps and are suitable for use in many different applications that require clean water to be delivered from a cold water storage tank, such as when boosting to pressurised hot and cold water systems, irrigation systems and above ground storage tanks and water transfer applications.

Offering many features and benefits, the family covers flow rates of up to 17m3/hr and a max of 9 bar. Of their many pluses are their compact size and the fact that they are simple to set up and use. Additionally they are quiet in operation and have built-in motor protection. They are suitable for potable water – and are fully WRAS approved.

With the flexibility to be used in a range of domestic and light commercial applications, these Grundfos booster family members have been very well received by the market and they are continuing to gain in popularity. This is no real surprise as they deliver flexible boosting solutions in one small, reliable compact unit.





    Facebook Twitter LinkedIn Technorati