Grundfos Hydro MPC booster sets gain WRAS approval

29/05/2013

Hydro MPC-E WRAS approval

Grundfos Pumps have recently attained WRAS (Water Regulations Advisory Scheme) full product approval status for their range of Hydro MPC E/F/S booster sets. This approval is only granted following rigorous mechanical testing and ensures that these complete booster sets comply with the various strict byelaw regulations and requirements as they currently exist in the UK.

The scope of this recent approval covers Grundfos Hydro booster families that comprise of between two to six pumps, are up to a 16 bar PN rating and pump models up to CR(E)90.

Over the years, Grundfos have built up a great reputation in supplying booster sets to the highest standards. With all the elements relating to the design, engineering and build combining to deliver to the most exacting standards, these sturdy, yet compact sets are perfect for a wide range of applications from hotels to education establishments, high rise developments to industrial demands as well as within the water utility industry itself.

The extra assurance this approval provides, is yet another reason to choose Grundfos to give your business the boost it may need.

Product information