Grundfos MAGNA3 plus MAGNA1 = the right answer

12/06/2013

MAGNA1 MAGNA3

Many changes have taken place within the circulator market in recent years. New generation pumps offer a range of benefits not least of all as they save significant amounts of energy. Grundfos have been at the forefront of these innovations.

Today Grundfos can offer both new and refurbishment projects an extended range of commercial circulators via the Grundfos MAGNA3, first introduced in 2012 and now the new MAGNA1. The family is designed for circulating liquids in a wide range of light commercial and commercial applications including heating systems, domestic water systems, air conditioning and cooling systems.

 

The MAGNA3 range delivers medium and large circulator pumps that come complete with electronically controlled motors based on permanent magnet (PM) and compact stator technology. They are now joined by the MAGNA1 circulator range that also delivers high energy efficiency, but with a reduced set of features. This makes them the ideal solution in a refurbishment situation or where you need to either replace a Grundfos UPS product or one of the smaller models from the original Magna family.

 

MAGNA3 and MAGNA1 pumps offer new products that have set the pace in the circulator pump industry by already meeting the Energy Efficiency Index (EEI) level set for 2015. You can trust Grundfos to give you an answer that will add up.

Find out more about MAGNA3 and MAGNA1





    Facebook Twitter LinkedIn Technorati