Grundfos MQ the compact pressure booster

05/08/2013

MQ

The Grundfos MQ booster system is a fully integrated unit that delivers a complete water supply solution. These systems come complete with a pump, motor, diaphragm tank, non-return valve and pump control. With everything available as a single unit, this means the unit comes ready to install.

Once filled with water MQ units can guarantee lifting from a depth as low as 8 metres. The innovative water-cooled motors also mean silent operation and the integrated components deliver premium performance.

 

So whether the requirement is to pump water from a well or to increase mains pressure via a break tank or the mains depending on local water authority rules, with over 1 million MQ units in use around the world these solutions have already proved their value.

 





    Facebook Twitter LinkedIn Technorati