Grundfos SOLOLIFT2 is second to none

04/12/2012

Macerator

The revolutionary SOLOLIFT2 is a range of sewage and wastewater domestic lifting stations from Grundfos. The family comprises of just 5 models that, through the flexibility of their design, their adaptability and performance provide the solution to handling wastewater for any combination of WC, bidet, sink, shower and washing machine.

They can be used in a wide variety of applications: where there is a requirement for an extra bathroom, for a basement installation, in holiday cottages, for adding facilities in hotels and guest houses, adding facilities for the elderly or the disabled or during the renovation of offices and other commercial buildings.

The modular design of today’s new Grundfos SOLOLIFT2 macerators ensures the servicing can normally be achieved in situ without the need to drain down the system. Additionally SOLOLIFT2 models are not only suitable for new installations but also for replacing an existing unit and also offer the option of either horizontal or vertical discharge connection to a variety of discharge pipe sizes.

In total the updated range incorporated 15 new features some of which are unique - that puts them ahead of competitor models. The SOLOLIFT2 has been very well received and Grundfos are pleased that the product has been not only readily accepted but embraced as a significant improvement and that today many installers and customers recognise that the Grundfos SOLOLIFT2 is second to none.

 





    Facebook Twitter LinkedIn Technorati