New B&Q store chooses Grundfos packaged fire suppression system

04/09/2013

Packaged Pump House solution

B&Q is the largest DIY and garden retailer in the UK with 350+ stores within its portfolio. They are continuing to expand and recently opened a new store in Burgess Hill, Sussex.

With a stock profile that encompasses around 40,000 lines - many of which are flammable - a state of the art fire suppression system is a high priority for B&Q. This is why fire specialists Grundfos Pumps worked in conjunction with Alpine Fire engineers to develop a bespoke solution. They subsequently proposed a Grundfos Packaged Pump House solution that would meet the most stringent criteria.

 

Grundfos introduced these systems in 2009 and each pre-packaged pump house is delivered to site complete with the pumps – in this instance 2 x LPCB high hazard diesel pumps - and with the necessary pipework, valves, wiring, heating, lighting and drainage, all packaged within in an insulated steel enclosure and mounted on a structural steel baseplate.

 

Packaged fire units from Grundfos offer several key benefits: reduced labour requirements/costs on site, reduced ground-works, all are fully assembled and pre-tested in a quality controlled environment at the Grundfos factory and Fire Excellence Centre in Sunderland, prior to delivery.

 

Fully compliant with the BS EN12845 installation standard and delivered crane-offloaded to site; this solution is one neat package that will continue to deliver for many years to come.

Learn more about Grundfos Fire Protection

Visit the packaged pump house product page

Download sales leaflet for Grundfos packaged pump houses  





    Facebook Twitter LinkedIn Technorati