Dundee get the fire power

Overview_TEXT

Overview

Dundee Airport is located in the heart of Scotland and is only 2 miles from the city centre.

This regional airport offers daily services to London City Airport, making it ideally positioned to serve both the business community and tourist industry, especially as St Andrews, Gleneagles and Carnoustie golf courses are all within easy reach.

As with any airport, safety is the highest priority, and regular exercises are routinely undertaken to ensure that in the unlikely event of an emergency the correct back up is available. Grundfos Pumps recently provided the site with a 3-pump Hydro booster set that provides the water required to the fire rig.

Grundfos worked on this project in partnership with Pump Action who undertook the installation and provided the weatherproof enclosure and cold-water storage tank, for the client - Dundee City Council.

The booster set has a dual purpose as it is being used to supply the water needed to meet the strict fire fighting safety exercises that are a regular part of the overall airport safety regime as well as for filling the fire trucks with their 10,000-litre water capacity in 5 minutes.

We all hope the set will never be needed for a ‘real’ fire situation, but should it be, we know it will deliver.






    Facebook Twitter LinkedIn Technorati

Topic:

Commerical Building Services

Location:

Dundee - Scotland

Company:

Dundee Airport

Related Products_TEXT
Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Telephone

01-4089800

Fax

01-4569459

Address

Unit A Merrywell Business Park
Ballymount Road Lower
Dublin 12
D12 PW56

Contact

If you need a similar solution, please contact us for further information.

Telephone

01-4089800

Fax

01-4569459

Address

Unit A Merrywell Business Park
Ballymount Road Lower
Dublin 12
D12 PW56