Girvan Community Hospital

Overview_TEXT

Overview

A new £21.5m hospital project is now nearing completion and when it opens its doors later this year it will provide a range of services for residents of Girvan and the surrounding South Ayrshire area.

This latest health project that has been designed to deliver health services right to the heart of the local community and facilities will include: in-patient services, a rehabilitation unit, a casualty department as well as other outpatient services. All of this will be combined with two existing general practices – all under one roof.

Working with consultant RSP Consulting from Glasgow and contractors James Frew Ltd, Grundfos Pumps have delivered a wide range of pump solutions that have been designed to ensure the best pump related back-up solution is available to the community.

To meet the high efficiency standards the project demanded, the M+E solution includes a wide range of energy efficient Grundfos pumps. Performing their role in this solution are members of the Grundfos TPE(D) family of single stage centrifugal pumps; UPE circulator family, IMpress pressurisation sets and incorporating a range of energy efficient CRiE pumps- two booster sets – one to ensure that demand for water is met and the second to provide a rain water solution to augment mains supplies.

Delivering health to the heart of local communities has been proven to save life’s and Grundfos are delighted to be part of this initiative.


    Facebook Twitter LinkedIn Technorati

Topic:

...

Location:

Girvan - Scotland

Company:

.....

Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Telephone

01-4089800

Fax

01-4569459

Address

Unit A Merrywell Business Park
Ballymount Road Lower
Dublin 12
D12 PW56

Contact

If you need a similar solution, please contact us for further information.

Telephone

01-4089800

Fax

01-4569459

Address

Unit A Merrywell Business Park
Ballymount Road Lower
Dublin 12
D12 PW56