Fire Protection

Overview

Overview

When you think of manufacturers and suppliers of fire sets, the Grundfos name may not be the first name which sprang to mind, however today we offer the world’s largest approved range of fire pumps and can provide a wide range of packaged and containerised systems that meet with NFPA, UL, FM standards as well as local LPCB (Loss Prevention Certification Board) certification. This means that Grundfos are the ideal partners to work with you to deliver a complete ‘one stop shop’ for fire pump solutions.

Within the UK, each building is given a designation that is defined by a number of criteria and given a hazard category. There are three of these (for LPCB systems) – light hazard, ordinary hazard and high hazard. These are dependant on the combustibility rate of the items within the building (for instance, a high combustibility would be considered a ‘High Hazard’.

Correct commissioning is always important, but for fire systems this is particularly so. It is vital that commissioning is undertaken by properly qualified personnel who will carry out a full range of tests to ensure that the set is fully compliant and meets specification.

 

See examples

 

 

Related applications
Contact
Local sales company

Telephone

01-4089800

Fax

01-4569459

Address

Unit A Merrywell Business Park
Ballymount Road Lower
Dublin 12
D12 PW56

Local service partner

Telephone

01-4089800

Fax

01-4569459

Address

Unit A Merrywell Business Park
Ballymount Road Lower
Dublin 12
D12 PW56