Showing 2041 to 2050 of 2150 results
UPA 15-90 N
The Grundfos UPA 15-90 N is a small stainless steel circulator pump designed for water pressure boosting in domestic properties to provide additional pressure to hot and cold water taps and similar outlet points.
UPS 15-50 hot water circulator
A traditional secondary hot water circulator. For secondary hot water distribution to circulate water in the system to ensure hot water is available on demand.
UPS2
The UPS2 is the ideal product for the replacement of small heating circulator designs which are currently installed in heating systems with limited space and which do not meet the current efficiency levels as stipulated under the EuP directive
UPS2 25-80 and 32-80
The latest additions to the Grundfos UPS2 circulator family of British built pumps the UPS2 25-80 and 32-80. These pumps have been specially designed to augment the current range and provide 8 metre options.