Boiler shunt
The primary task of the boiler shunt is to ensure that the difference in temperature between the top and the bottom of the boiler is not too high. A high temperature difference can cause tensions in the material and thus reduce the life of the boiler.
Brackish water
Brackish water is water that has more salinity than fresh water, but not as much as seawater.
Break Tank
Break tanks are implemented in boosting systems in order to supply the system if the mains supply becomes insufficient.
BTU (British Thermal Unit)
The British thermal unit (BTU) is a unit of energy used in the power, steam generation, heating and air-conditioning industries.
Buffer tank
A buffer tank is a storage tank used on the cold user side of an air-conditioning system.
Butterfly valve
A butterfly valve is from a family of valves called quarter-turn valves. The
Bypass connection
Pipe connection between the suction and discharge side of a booster set in order to bypass water when the pumps are not in operation.
Calculating heat loss
The calculated transmissions loss is the sum of the heat losses from each individual section of the building.
Calculating pressure loss
To select the right pump and achieve proper balance in the system, it is necessary to calculate the pressure loss throughout the system.
Calculation of flow
In order to calculate pressure loss in a heating or cooling system it is essential to know the volume flow rate Q.