Fire protection matters with Grundfos

06/05/2019

Fire protection matters with Grundfos

With 28 classrooms, an additional 4 nursery playrooms plus a library, all combined in a single modern unit, the recently opened Wallyford Primary School in East Lothian is ready to meet its School of the Future billing.

As you would expect, safety was an important factor that was integrated into every aspect and Grundfos Pumps were delighted to be involved with assisting in specifying and supplying a specialist pre-fabricated school pump house.  The OH1-15 single electric packaged pump house is fully compliant with all standards and technical bulletins.  With a compact footprint of just 2m x 2.5m these units arrive on site fully commissioned and ready to plug n’ pump. 

Fire safety is something very much in focus these days and Grundfos are ideally positioned to meet a wide range of fire requirements from compact domestic units, through ordinary and high hazard sets, FM/UL sets as well as a wide range of hydrants and wet risers. All fire sets are built in the UK and deliver a robust and cost-effective solution.

This new campus was built to meet a range of needs and is set to play a central role, not only in education but also in the wider community and Grundfos Pumps are pleased to be delivering the fire related peace of mind.