Grundfos deliver the power to shower

03/11/2019

Grundfos deliver the power to shower

Grundfos Pumps might be better known for their range of reliable circulators, but they also offer a wide range of other pump products, including an extensive shower pump portfolio. This shower pump range offers a wide selection of pumps that are designed to booster the water pressure to a shower or bathrooms fittings. There is a total of 5 models available, in various bar ratings from 1.5 to 6 bar.

So, whether you require a twin or single impeller, brass or composite, universal head or positive head operation – Grundfos will have the ideal pump to meet your needs. 

Single impeller pumps generally help boost the pressure of cold water supplied to a combi boiler while twin impeller pumps are used to boost the pressure of hot and cold water to a single shower, multiple showers or a whole domestic house system. For larger installations, such as showers in a sports facility, single impeller pumps can be used, and these can be placed on both hot and cold feeds and integrated with thermostatic shower valve protection. 

By working with a reputable shower pump manufacturer such as Grundfos, you can be assured that any shower pumps you install will be fit for purpose and will continue to deliver - taking the pressure off you.