Grundfos have the last word in end-suction pumps

05/04/2019

Grundfos have the last word in end-suction pumps

When you need to be able to rely on your end-suction pumps, look no further than Grundfos Pumps who are a proven, reliable, innovative name in delivering these solutions.

In their 40+ years of delivering these specific pump models, they have introduced many improvements that have enhanced both the product line-up and its application span.  This means that today solutions have the answer to water supply, industrial pressure boosting, industrial liquid transfer, HVAC and irrigation solution demands.

With an enviable reputation with their Grundfos NB(E), NGK(E), NK(E), NKG(E) ranges that are manufactured in ISO 9001 certified facilities, the range comprises of a comprehensive series of close-coupled (NB/NBE family) and long-coupled (NK/NKE family) pumps that are compliant with EN733 or ISO2858. All are non-self-priming single stage, centrifugal pumps with axial suction port, radial discharge port and horizontal shaft.

The handy back pull out design facilitates the removal of the motor, coupling, bearing bracket (NK/NKG) and impeller without disturbing the pump housing or pipework. This simplifies maintenance and enables servicing of even the largest pumps, by a single person with a crane. 

When you need an end-suction pump that has reliability, flexibility, energy efficiency inbuilt and that can work in a wide range of demanding environments – Grundfos have the answers often available on a short leadtime.