Grundfos CONLIFT when gravity needs a hand


Grundfos CONLIFT when gravity needs a hand

Condensate from dehumidifiers, air-conditioning systems, commercial cooling systems and condensing boilers can be a problem, when it cannot be removed by natural gravity. There is however, a straightforward solution provided by the Grundfos CONLIFT range.

Comprising of just 2 models; the CONLIFT1 and the CONLIFT1 LS, both variants are supplied with an integrated NC/NO contact and cable so that if the overflow switch detects a high-water level, this can be used to switch off the boiler.  

Their advanced design means they will operate automatically when condensate enters the collection tank from an appliance. The units then lift the condensate up to 5m in height and across a distance of several metres to the required drainage point. Another plus is that these units require minimal maintenance. The motor/pump unit can turn 180o on the tank which increases the flexibility of the installation process, a situation which is enhanced by the four symmetrical inlets that means the unit can be connected from any direction. 

Thanks to the modular system, both CONLIFT1 and 1 LS can be upgraded with either an alarm PCB and/or neutralisation unit which can be retrofitted in case changing conditions require this flexibility. Find out more about the CONLIFT family as well as other exciting new developments from Grundfos by visiting