One MAGNAificent performer

06/12/2018

MAGNA1

An updated and improved range of Grundfos MAGNA1 Model C pumps are now available in both single and twin-head circulator options. These circulators are suitable for use in a wide range of light commercial and commercial applications such as heating, air-conditioning & cooling and hot water circulation. Additionally, they offer the perfect solution in a refurbishment situation where there is a need to either replace a Grundfos UPS product or one of the smaller models from the original MAGNA family.

Besides the existing benefits of a simple user interface and best in class efficiency; these new models now offer the option to monitor the pump via a fault relay. Also, they offer a digital start/stop input that allows the pump to be monitored remotely; having a wireless function means that the popular twin-pump models will secure uninterrupted operation. 

This cost-effective range is a tried-and-tested replacement pump for buildings where reliability and efficiency are paramount and where BMS integration is required. Plus, there is a wireless function for twin-head pumps to maintain full flow if one pump is unavailable – meaning reduced downtime and continuous operation.

:: Get product details

:: Learn more about the MAGNA1 Model C