Right at home with the Grundfos FireSAFE

08/01/2020

Right at home with the Grundfos FireSAFE

The Grundfos FireSAFE domestic range delivers a compact, consumer and installer friendly response to the growing demand for domestic fire suppression systems as well as meeting the legislative demands that new homes in Wales must meet.

Designed to ensure flexible installation and easy maintenance, these models comply with BS9251:2014 and are WRAS approved. Each unit comprises of a dedicated controller and Grundfos CM pump mounted in a tamper resistant metal enclosure. The enclosure comes in two sizes, both of which are dimensioned for easy installation in domestic environments.

This range can be used in a variety of domestic installations including houses, apartments, sheltered and student accommodation, care homes and small hotels. Larger properties could benefit from specifying larger FireSAFE Residential products.

Offering a great range of features such as simple installation and commissioning, a compact size, minimal maintenance, combined with their advanced system controller and in-built self-test makes these the ideal solution in many situations.