The Grundfos UPS3 changing the game

06/10/2019

The Grundfos UPS3 changing the game

Since the launch of the UPS3 15-50/60, it has gained a significant following of supporters and those numbers are continuing to grow. One very important attribute is the reliability this pump can demonstrate, as it maintains a consistently high performance throughout the season. Improved energy efficiency is another key talent, that combined with an easier to wire plug and on-board diagnostics, really makes this pump stand out from standard offerings.

Peace of mind is guaranteed as this pump was built on a platform that was proven in millions of boilers, prior to its launch. 

The ALPHA1L is a circulator pump designed to be used in domestic heating systems for either variable or constant flow rates. This is because it automatically controls the differential pressure by adjusting the pump performance to the actual heating demand without the use of external components. 

All this means that when you need to combine reliability, efficiency, head, diagnostics and fitting time, there really is only one player to choose.
We all want to support the winning team and with so many great signings, joining forces with the Grundfos domestic circulator team, will ensure that you’ll be in a league of your own.