Grundfos MAGNA1 simply the smart choice

01/08/2018

Grundfos MAGNA1 simply the smart choice

Since the MAGNA family launched back in 2001, we have been constantly re-visiting the range to ensure that it continues to encompass the many demands that are required of a modern circulator and can be used in various applications.

Today, this has led to an improved range MAGNA1 Model C pumps that have recently been launched. These single and twin-head circulator options are designed for circulating liquids in a wide range of light commercial and commercial applications. This includes: heating systems; air conditioning and cooling systems; domestic water systems; ground-source heat pump systems and solar heating systems.

These pumps can offer the perfect solution in a refurbishment situation where you need to either replace a Grundfos UPS product or one of the smaller models from the original MAGNA family. They are designed for circulating liquids in heating systems with variable flows where it is desirable to optimise the settings of the pump duty point, thus reducing energy costs.  These latest generation MAGNA1 Model C pumps now can also provide for some basic communication options.

:: Download the MAGNA1 Model C brochure

:: Learn more with MAGNA1 ECADEMY training topic