End-of-Life Information
Grundfos Submersible Pumps (SP) must be disposed of according to local regulations by using a public or private waste collection service. If this is not possible, contact the nearest Grundfos company or service workshop.

Safety Risk

  • Safety related to materials used
    There is no risk for people during the disassembly process posed by the materials used in the product.
    Be sure that the Submersible pump is clean and empty for liquid before disassembly.
  • Safety related to handling the product
    Care should be taken when handling the pump/components due to the weight.


Disassembly of the Product
The main materials of the components are:

  • Stainless steel (plate, round bar and cast)
  • NBR/FKM rubber

SP can therefore be recycled to a large extend – depending on the national possibilities for recycling.

To disassemble a SP pump you need special tools, please see the SP service instruction.

“The service instruction is available on www.grundfos.com/webcaps”

Pos. no.Designation 
MaterialSpecial disassembly considerations
1Suction interconnectorCast stainless steel 
2ShaftRound bar stainless steel 
3Spacing washer  Carbon   
4Seal ringNBR/FKM 
5Impeller completePlate stainless steel 
7Chamber completePlate stainless steel 
8Valve Cup with guidePlate stainless steel 
9Valve casingCast stainless steel 
10Cable guardPlate stainless steel 
11Strap completePlate stainless steel 
Additional materials:Screws, nuts etc.: Various materials less than 5 % of weight.
6a SP_explode-1